5G NR

Using Custom Payload Data

You can apply custom payload data to the following channel types: SS/PBCH, DL-SCH, DCI and UCI, UL-SCH. Select either Custom Pattern or User File from the Payload Data Type menu.

Custom Pattern allows you to create, load, and save custom payload data directly in the software's editing field.

User File allows you to apply an existing custom payload data text file.

The list below describes some of the common behaviors and couplings associated with custom payload data.

Carrier Downlink

Carrier Uplink